[ LP8860-Q1 ] Low Vin Operation
Hi,
When I evaluate LP8860Q1-EVM together with LED Load Board, and decrease the input voltage, from certain Vin, LED start flashing and Boost Overcurrent Fault is toggled. Here is my test conditions.
- LP8860-Q1EVM
- J8 is VBUS (LP8860-Q1 VDD is supplied from VBUS)
- LED Load Board with 8series/4strings
- Boost Frequency: 303.45KHz w/ and w/o Spread Spectrum
- Brightness: 100% with 150mA current scale
On this condition, when Vin reach to around 12.3V(w/o SS) / 12.7V(w/ SS), LED start flashing.
Can you help me to understand why this happen?
I need to reduce Vin further down to 4.5V as system requirement.
Thank you for your support in advance.
Regards,
Ken