Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8860-Q1 with minimum external components

Hi,

I followed Figure 66 in the datasheet to design a solution with minimum external components. The 4 LED strings were not lit.

I measured, VLED+ was 30V, which 36.6V/360mA was suppose to be normal. OUT 1 to 4 were about 4V. FAULT was 5V high logic. EN was set 5V. The input frequency on PWM dimming pin was 200Hz.

It did not help,if I reset the NSS. Could you help check my SCH to find out why it was not lit?

Thanks.