Other Parts Discussed in Thread: LM5021-Q1
Team,
Please tell me about the following inquiries of LM5021-Q1 from customer(TDK).
1. On 1st page(Features) of DS, there is the following description about the temparature range.
"– Device Temperature Grade 1: –40°C to 125°C Ambient Operating Temperature Range"
but, in the recommendede operation conditions, it has been specified as –40°C to 125°C for Junction temperature.
The Junction temperature range is correct?
2. The peak source(IO_SRC) & sink current(IO_SNK) of OUT have been specified as 0.3A/0.7A of typical value only.
Customer would like to know the minimum value for them. Can you show it?
If it is impossible, Can you show the distrubuted data of both patameters over some lots?
Best regards,
Hidekazu Someno