We want to use one LP2980AIM5-3.3 as supply for an analog circuit (IL = 21 mA). The used temperature range is from 10 °C to 60 °C and we need an accuracy of at least 0.9%. In the datasheet (6.5 Electrical Characteristics) I can only find Information over the whole temperature range.
What is the accuracy of the device in the needed temperature range? Is there any detailed information?
Thank you!