Hi
I have made a PCBA board using bq40z60 chip. the schematic is exactly same with the bq40z60EVM-578 .
I used 3 cell batter (BRC18650 5000 mAh 3.7v li-ion ). I have connected the board through EV2300 to the Battery Management Studio 1.3.42.
Everything is OK, but it looks the chip's default setting is not working as Evaluation Module ( the charger and discharge and LED are not working).
I just want to let the board works like Evaluation Module (has basic charge, discharge, LED and protection functions).
Where can I found the Settings for Evaluation Module (bq40z60EVM-578) or some one has settings for this Module?
Attached is my board settings and .gg file.
Thanks very much.
Jun P,
Streambox inc. Seattle, WA. USA