Hi team,
I am currently working with the LM25011 and we have a relatively wide range for the load from 700 mA to 100 mA at 15V. At low power, we are seeing a lot of noise at the output and the IC goes into discontinuous mode. Do we have any remedies for this and/or any other ICs that might be better for this application supporting the wide load range? The input voltage range here is 24V to 40V.