Hi, I need to implement active balancing for a battery bank having 27 Li-ion cells with a capacity of 15600mAh and a total voltage of 100V. I read about bq78pl114 but it is just for 12 cells and it is not recommended for Li-PO batteries which I could use in a future. Reading another forum it was recommended to use EMB1428 and EMB1499 as a solution for active balancing, but it is needed to implement the balancing algorithm, I would like to use one algorithm based on individual SOC of each cell, which would be the better solution? I think there must be an smarter way than using bq34z100 for each cell could you help me please?
Another question, why the battery capacitty determines the right IC gauge?, my application is for EV but there a lot of IC with SOC estimation for batteries having 16000 mAh using impedance track technology but they are intended to be used in portable electronics, but impendance track is not found for IC intended for batteries with a capacity above 32000mAh.
Thanks a lot