[ UCC28880 ] Low Side Buck Configuration for Dynamo
Hi,
Do you have any ideas whether UCC28880 is suitable for dynamo to have stable DC output voltage? The input voltage from dynamo is something like +/-100V (200Vpp) with various frequency (it's depend on rotation number).
The frequency is different(not 50Hz/60Hz) from AC input, however it seems the PMP8509 is a similar configuration to what I want.
Since I just start studying this , so I'm sorry that I cannot give enough information.
It's really helpful if you can share your ideas.
Thanks,
Ken