I'm planning to do a redesign using the LM3150 with a very variable load. The load will be in the range of 0 (few mA) up to 7A, all at 27V. The unit will have an input voltage of 36V (very stable). The load will not shift rapidly!
Anyone who have any experience of similar designs with the LM3150? Are there any better options than the LM3150?
Regards,
/Lowe