Hello,
I would like to know if the Coss related losses are encountered for ZVS phase shift converters. I read some articles, from several suppliers, that are highlighting the need of counting these losses too. However, in UCC28950 application guide these losses are omitted and many other suppliers are saying the other way around - that the losses do not exist due to resonant charge/discharge of the capacitance. My belief is that there are some losses due to the fact that the resonating inductance must provide the required energy for soft switching (even if through resonance). However, I do not have the grasp on the subject to know if this energy is practically dumped within the resonating tank, or is rail recovered (as the body diode clamps the switching node to rail voltage prior to on transition). Even if the losses are low in comparison to turn-off or conduction losses, I would like to know just for my general knowledge if the Coss losses exist or the entire energy is recovered.
Many thanks for your support!