Hi,
The primary magnetizing inductance for the power transformer is calculated in UCC28950 application note in eq. 9 page 3. I presume the 0.5 term within the denominator comes from half the switching frequency of the output inductor (the operational frequency of the transformer) and is better linked to fs rather than the output ripple inductor current - please correct me if wrong.
In eq. 17 page 5 the primary magnetizing current is determined based on output inductor frequency. Is this ok? I believe that we have to consider the transformer operatig frequency as it is a transformer parameter. Is it possible to find how the formula is derived (both: eq. 9 and 17)?
Also this parameter is used to set the sensing network for the current transformer, so is quite important to know the correct value. I believe the IP1 term in eq. 85 page 15 is similar to IPP term in 18 page 5 - please confirm!
UCC28950 application note link: http://www.ti.com/lit/an/slua560c/slua560c.pdf
Thank you!