Hello,
The next firmware release for BQ78350 was planned for October.
Do you have any update?
Regards,
Frederic
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using bq78350-R1 latest firmware with BQ78350-R1 chip on bq769306EVM. NCR186050B(3350mah) cells are connected to EVM.
Configured EDV2, EDV1 and EDV0 to 3215,2800,2500 respectively and enabled compensation EDV.
BQ78350 always took EDV2 as aproximately as 3500 and reduced the learned FCC to aproximately half. Waited for 15 cycles, but it settled at FCC at 1700mah.
I guess BQ78350 is not taking EDV values from the CEDV cfg registers. Kindly help me in figuring out issue.
Thanks Onyx,
I was referring to the email gpc_support@list.ti.com which seems to bounce back any email I send to.
Thanks,