Hello all,
I try to do a learning cycle, but the discharge is stopped automatically before the threshold I choose, do you have any clues?
All the flag not show are 0 except ITEN, on the last line.
The data memory:
test.gg.zip
An another little question...is the BQ40Z60 able to do cell balancing during charging?I have a relatively strong cell unbalance when the charging voltage is near the maximum and the charger stop with a COV error. For example, I need to program a 3,5V setting voltage (I use LIFePo4) whereas the cut-off is 3,65V if I want a normal charge termination.
I also have a similar phenomenon on discharge with CUV, but it is less important to me.
Best regards,
Wilfrid