This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Parallel charging IC

Hello

The application requires implementing two Li-NMC battery (2600mAh each), to give a higher current output to the system.

The product selection guide has option for series cells configuration and not for any parallel config, which is also a fairly common use case.

Please suggest a suitable IC or IC matching closely to this configuration

- Each cell charges at more than 1A

- Combined Output from the battery unit

- Temp and battery monitoring

- Single USB/AC input for charging and preferably 2 USB outputs

- Analog controlled.

Thanks.