This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About DC/DC 12V/6.6A use TPS40210 with UCC24630 problem

Other Parts Discussed in Thread: TPS40210, UCC24630

I have power module 12V/ 6.6A use TPS40210 ( frequency setting 150kHz )  with UCC24630,

when i test power of performance by setting Electronic Load  CC mode, 0.5A~5A is OK,

but excess 5A UCC24630 DRV is off, Why?