Hello-
We are using TPS2511 USB charger in our design. There is a current limit and hiccup mode capabilities in that chip. It seems like due to the hiccup mode, current limit actually sets over current limit. What I mean by that is, if the current limit is set at 680 mA and we try to pull more the USB turns off instead of limiting the current. I believe what happens is we try to pull more current than the limit, voltage reduces below hiccup mode threshold of 3.8V, and device enters hiccup mode (turns off). Is this correct? If not what is the explanation for this behavior?
Thanks and Best Regards,
-Tim Starr on behalf of RK@ec