The data sheet for the Bq27510 indicates that the value for StateofCharge should always reside in the range from 0 to 100. Our system is reading out 120% for our stateofcharge on all newly received (10/2015) systems once assembled and programmed.
This poses a problem because the currently deployed firmware checks to make sure the value is between 0% and 100%.
What could cause the issue where the stateofcharge is 120?
Stats:
- Lithium Ion
- battery capacity is 1750 mAh
- charge voltage is 4.2