This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54560 power supply transfer function

Other Parts Discussed in Thread: TPS54560


I have a few of these out and they seem to be working like a champ. I'm just trying to make sense of the transfer function that was generated in web wrench. The web wrench design is given as Design : 1185265/43. 

The poles and zeros are given as:

Pole1 : 1.32kHz

Complex Pole: 4.09kHz  zeta=0.2393


Zero 1  : 4.09KHz


Zero 2 : 26.53kHz

The complex pole, and zero 2 can easily be explained by the RLC circuit placed on the output of the switch, but I can't figure out where pole 1 and zero 1 come from. Are they something that is internal to the tps54560 converter? Do they come from some sort of specialize analysis peculiar to switching converters?

I'm not having any trouble with these now, but I think it would be useful to understand this so I can avoid troubles in the future.

Thanks

Steve H