This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65072 could not charge the battery sometimes

Other Parts Discussed in Thread: DM3730, TPS65072

We are seeing some weird behaviour. Our configuration is:

DM3730 GPIOs is controller the PB_IN and PWRON.

DM3730 I2C is used to control the PMIC.

When we have a battery below 3.0V, DM3730 won't power up. So it leave PB_IN and PWRON floating. We had pulldown on PWRON and pull up on PB_IN.  Sometimes, TPS65072 could not charge the battery. Looks like the charge function is not activated even the AC is in (5V).

If the voltage is above 3.0V, DM3730 could power up and then issue PB_IN and PWRON. We don't see this issue. Should charger function always on when AC is in?

I had tested demo board and found the following truth table. I could not find any definition in the spec. In short, what condition could stop the PMIC from charging the battery( other than short, thermal, no battery)

PB_IN  PWRON    charger  Vsys

1                0                  On          On

1                1                 On            Off

0                 0                On            Off

0                 1                  Off            Off

  • Let me simplify the question:

    a. Is the charging circuit always enabled when valid AC is inserted, regardless of other pins state, such as PB_IN, PWRON, 

    b. Is there a latching state that charging circuit won't detect battery anymore?

    c. Under what condition that I2C access is not available?