Hi Guys,
I am working on a small voltage step down circuit using the LM317T.
Input voltage : 19VDC
Input current : 2A
Desired Output voltage( from LM317T) : 13.8VDC
I am using this circuit design :
Yesterday, i did testing with a solar panel & it burnt my filter cap( C2 ) at the output side. (probably of high current i guess).
Question is : What's the MAXIMUM INPUT CURRENT ALLOWED into the LM317T IC?