Evaluation Kit: BQ78PL114
BQ wizard version: 2.5.7
Firmware version: 5000 (CRC: 0x4104)
I am trying to track charge and discharge current from BQ wizard. But I am facing strange issue. As soon as I open BQ wizard on PC both charge and discharge FETs are turning Off. And I am not able to observe current on BQ wizard.
Following are steps
1) Connect battery to EVM (28 V)
2) Connect charger voltage (32 V)
3) Charge FET is ON, and 500 mAmp charge current
4) Connect USB to GPIO adapter to kit
5) Open BQ Wizard
6) No charge current, No voltage at PACK+ and PACK –
Anybody faced similar issue with BQ Wizard?
Is there any special configuration to allow normal charge/discharge FET operation with BQ wizard?