Hello everybody,
I created a golden Image for a bq20z80 batterypack. After the learning cycles completed, I noticed that some R_a values in the .gg-file were zero: e.g. "Cell1 R_a 0 = 0".
I wonder if such values could be correct. From what I know of lithium-ion batteries, they have impedances > 0 mΩ in the usually examined frequency regions. So are these zero values only a matter of the underlying algorithm and perfectly fine? Or could they lead to problems in the gauging calculations later on?
At the moment, the SOC values I receive from the battery seem reasonable that is.
Thanks,
Sebastian