I purchase the bq24610EVM (HPA422 REV. B) . The documentation however implies that it is for multi-cell applications, the question I have pertains to the connection of the cells to the EVM board. I will be using LiPo's @ 3500 mAh in a 6s1p configuration. The schematic & documentation for the EVM provides no information as to connection of cell balancing / cells in series, single, or parallel configuration . Is balancing not required, and am I to series the batteries and connect the series output of the batteries (22.2VDC~) to VBAT and GND? Some guidance needed.???