Hello,
can I ask you for hint how to run OTG mode on bq25895 ?
I´m working with bq25895EVM and I cant to run OTG until USB/VBUS is powered in.
Only when I use OTG pull-down then battery voltage is applied, but no OTG fuction run.
THX for help!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
can I ask you for hint how to run OTG mode on bq25895 ?
I´m working with bq25895EVM and I cant to run OTG until USB/VBUS is powered in.
Only when I use OTG pull-down then battery voltage is applied, but no OTG fuction run.
THX for help!
Hello Jeff,
thank you for respond. Problem is that I cannot get BAT above BATLOWV, because if no VBUS is applied, ADC is no working on bq25895 - Am I right? When I set "Start ADC bit" nothing happen and in status register is still 2.304 V. Is there any special ADC handling without VBUS input?
BR