This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MC33063A Questions

Other Parts Discussed in Thread: MC33063A

Hello there,

Below are my questions regarding the application for the MC33063A device;

From data sheet of MC33063A Figure 11, Page 15: When plug in values of R1 = 1.2K and R2 = 3.8K the Vo = 5.2V instead of 5V.

If Vin fluctuate between 24-40 VDC will this affect the 5V regulation? The reason I ask this question because I try to use the filter output from the secondary output of 24VAC transformer. The output could vary between 18-30VAC. this roughly equal to 24-40VDC after filter.

Thanks,

Tim Ta