We're using bqWizard 2.5.18 and FW5000 in our bq78PL114S12's.
Is the Pack Dynamic tab's Idle Timer parameter functional? It's never gone past 0 seconds for us.
Is the Pack History tab's Lifetime Delivered Amp Hours parameter functional? Or does it only increment to 1Ah after 10Ah are passed since the current values are 0.1x with FW5000?
Is the Pack History tab's Lifetime Maximum Power parameter functional? It seems to change with the existing conditions instead of displaying the max power level the chip has seen.
Thanks!