Hello TI,
The datasheet states the total input current when the device is OFF and also in STANDBY. What I’d like to know is, what is the supply current for the IN_BIAS rail and IN_BU rail when the device is ON? What supply rail(s) are needed to power up the digital control portion of the IC? I’m looking at providing a low-current “always on” 3.3V regulator for just those portions of the IC, and providing a higher-current 5V supply for the LDOs and DC/DC converters. Can I do this? Do they have to be the same voltage?
Thanks,
Dan