This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I`m using LM5050-1 for Oring FET controller.
In evaluation board I see the problem with LM5050 OFF signal.
i conected power supply with VIN 12V, Vout is also 12V , even I connect to OFF TP voltage 2-5V.
When OFF signal connected to 0V the Gate voltage is 23V, when I connect 5V (expected Vout=0V) to OFF TP, the Gate voltage is 12V and Vout is 12V.
Thanks,
Igor