This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH08T260 - variable resistor as Rset (Vo Adjust) with maximum current 4mA.

Hi,

I would like to use TI module PTH08T260 and set output voltage using a variable resistor that works up to 4mA only. This would be connected as Rset is shown in the datasheet. Info about power of Rset is presented in the datasheet, but no needed info about Vo Adjust pin. I need to understand how to calculate the range of resistance values that are acceptable taking into account the maximum continuous current restriction (4ma max). I will appreciate advice as soon as possible.

Thank you,

Zar