This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1 - Maximum Distance PbA Battery terminals for reliable measurement

Other Parts Discussed in Thread: BQ34Z100-G1, BQ34Z100

Hi,

Typically automotive batteries are placed under the hood and the temperature level there is usually beyond the standard 85 degree C.

I am considering the option of keeping the device and electronics inside the cabin - about 1 to 2 m of cabling from the device.

Kindly guide me whether it is OK to do so.

What is the maximum distance PbA Battery terminals from BQ34Z100-G1 for reliable gaging/ measurement.

Also please advice me whether there is any automotive grade version of BQ34Z100-G1.

thanks and regards,
-Sreekumar