For the TPS65930, we're trying to interpret the load capacitance requirement for the KPD.Cx pins, given in Table 3-4 of the datasheet.
The table lists "Load (pF) Output Mode" as 30 pF for each column output. Is this the maximum allowed line capacitance, or is this the capacitance of the output"
Put another way, the keyboard row inputs specify a max rise/fall time of 3051.8ns. Can my system capacitive load exceed 30pF as long as I do not violate these rise/fall times?
Thanks!