Greetings ESC. My customer is using the TPS61170 as a boost driver to drive an LED string for optical measurement.However, he is having a challenge with the ripple and needs suggestions. the following is the description. Please advise.
"The receiver (photodiode) has a large gain, therefore, I want the LED light to be as stable as possible so we don’t see the fluctuation at the photodiode output. I though TPS61170 will be a good choice, but I ran into the problem as follows:
Requirement:
- Voltage input to TPS61170: 3.3V
- Voltage output from TPS61170: 3.3V to 18V
- PWM voltage control : 10% -90% duty cycle
- Current requirement: 250mA
- Adjustable drive LED voltage: 3.5V to 18V
- Change R1 on the eval. board to 100K
Problem
- Get 50mv ripple at low current around 10mA at 25%duty cycle, output voltage~3.7. I can live with it
- Increase the PWM to 35% - current output of the TPS61170 is fluctuated – from 100mA to 200mA
- Increase more than 40%, Voltage output is swinging ~ 4V
My question:
- Can we use this chip to drive the LED using PWM to increase the voltage from 3.3V to 18V?
- We also want to drive the TEC ( Peltier) in the same way. 0.5V to 5V – 0.9A max