Is there any IC which converts +12V to -12V like TPS60403(+5V to -5V)???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There are any number of converters that will convert +12 V to -12 V. That topology is inverting buck boost. Depending on your required current you might start with TPS54160:
You can use this technique for any device in that family.
I do not directly support those devices. You should be able to design your circuit based on the reference materials provided. Can you tell me about your application?
The power that I need to design apply to Preamplifier op amps of ECG signal acquisition module.It need -12V@2A.I think the circuits that WEBENCH designed is
complex and I plan to use PTN7860A.However,if there are other converts like TPS54160A which is cheaper,I think it will be better!