Hi,
I'm using the TPS61200-EVM with a solar module(3W, max 5V) as source and a 35F / 2.7V Supercap as output.
UVLO-Divider is set to 3V switch on.
At low light condition the device stucks with a VIN-voltage of .25V. But VAUX remains at 1-1.8V.
Even when I remove the solar module VAUX is still at this level.
Is VAUX supplied from Supercap through VOUT-pin?
Should the UVLO setting prevent the IC to stuck at such low input voltage?
When I connect the solar module directly to VIN , "behind" the 100Ohm resistor, the device tends not to stuck. What is the reason?
Thanks for help, best regards