This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LED driver

Other Parts Discussed in Thread: LM3421

Hi Ti,

Looking for a preferably an Automotive part if there is nothing we are ok with a stranded part.

specifications are:

VIN: 8-30V... Minimum could be increased to 10V

VOUT: 21-26V (This is based of 6 IR LEDs with a max Vf of 4.3V

IOUT: 2A... This is not a continuous current but is pulsed for 2ms every 16.5ms,

Sujeeva Wettasinghe

Avnet FAE