I am having issues with the 12V to 20V 4A boost controller circuit that I have designed using the LM3478. I used the guidance of the LM3478 datasheet and AN-1286 Compensation for the LM3478 Boost Controller. The issue is that the output voltage drops from 20V unloaded to 17V loaded with a 5ohm 200W resistor trying to pull 4A. Also, the output is very noisy when loaded down. The circuit can source 2A without any noticeable voltage drop on the output. Also, the AC-DC converter can source over 8 amps of current. Below is the list of components that I have used for my circuit. Please refer to the LM3478 datasheet Figure 27 for the references.
Vin - Cosel TUNS100F12 12/100W ACDC Converter
Cin - AVX TPSD107M020R0085 100uF (2 EA), TDK C1608X7R1H104K080AA 0.1uF
L - Wurth 7447709150 15uH
D - Diodes Inc. PDS1040-13 Schottky Diode
Q1 - Vishay SI4420BDY-T1-E3, N-Channel MOSFET
Cout - AVX TPSV107K025R0100 100uF (2 EA)
Rfa - 39.2Kohms (for 400KHz) Rf1 - 120Kohms Rf2 - 7.87Kohms
Rsn - Vishay WSL2816R0200FEH 0.02ohm
Csn - 0.01uF
Rsl - 0ohms
Rc - 1.3Kohms
Cc - 0.15uF
My calculated poles and zeros for a 4A load
fz1 = 15.9KHz
fz2 = 18.6KHz
fz3 = 816Hz
fp1 - 155.2Hz
fp2 - 21.2Hz
I would appreciate any insight or recommendations. Please advise. Thanks.