Hi,
My application uses USB 2.0 as input into my system. System loads are 3.3V @ 1A and 5V @ 2A. So I will need to use two TPS82084s . Please let me know :
Q1. If the USB 5Vin and Vout=5V OK to do with TPS82084 ( as data sheet indicates Vout can be up to Vin).
Q2. If the USB 2.0 spec states 500mA max draw, what would be the ripple current to draw 1A@3.3V and 2A@5V.
Q3. if the TPS82084 is not a good match is the tps542941 a better device?
Thanks