This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About TPS23753 SW Coli change to Other Coil and dose we have side effect ??

Other Parts Discussed in Thread: TPS23753, TPS23753AEVM-004, TPS23753A, PMP7355

Hello 

Now we started to PoE production  with TPS23753.

 Our spec is  5V / 2A(10W) output. 

EVM reference recommended coil type is   "  HA3803-BL  " . 

 *  Reference  EVM  Type is TPS23753AEVM-004 

But we did not use same  EVM Reference coil.

Now we used this coil   " POE13F-50L"  for our product. 

a) EVM Refarnce and Recommend  Coil   * Both  is Coil Craft . 

  HA3803-BL       datasheet.octopart.com/HA3802-BLB-Coilcraft-datasheet-22122339.pdf

         

b) Our using Coil           

  POE13F-50L_ 3   data Sheet   pdf1.alldatasheet.jp/.../POE13F-50L.html

【 Question 】

 We worry about some one side effect  and some other issues.

 Could you give us some comment when  use this "  Not Reference coil   for " TPS23753A ??

We understood this question is very hard question and difficult answer .

Please give us everything comment to us .

Thanks and Regard

Jasper  ( Japan Disty ) 

 

   

  • Hi Jasper,

    If using the POE13F-50L, does this mean you are designing with a diode on the secondary? I recommend looking at PMP7355 as a reference when using this transformer with the TPS23753A. There are not too many differences and mostly only component values differences.

    Thanks!
    Regards,
    Darwin