Hello,
i want to use the mosfet CSD19536KCS for a motor system. When i read the datasheet i find some questions.
Figure 7: if Tc=125°C, Id=100A, then Rds(on)=4mohm
Now Vds=100A*4mohm=0.4V
Figrure 10 (SOA): when Vds=0.4V, Id=65A<100A.
Figure 12: when Tc<125°C, the max. Id=150A.
These figures dont match togehter. Is there something wrong with the SOA or the resistance Rds?
And i try to simulate this model using LTspice. In the Pspice model library there are only 4 nodes. I think it should be 5: Gate Source Drain Tj Tc.
So anbody can tell me how to solve it? Kindly explain.
best regards,
Qiu