Hello,
We're using TPS63002 to generate 5v / 0.5A (peak) from Li-ION battery (see below schematics)
We see that the device is damaged in high percentage ~40%!!! in production.
In a functional circuit, we can see 5v on VOUT_5V and measure large resistance [Kohm] between L22 and GND.
In failing circuit the VOUT_5V is at 2.3V and we see short ~58 [ohm] between L22 and GND, in parallel to high current consumption.
manually removing each device and soldering a new one solves the issue permanently.
We've manufactured ~70 units till now.
Any idea what might be wrong ????
Any replacement IC that might not be that sensitive???
Thanks in advance for your help!
Gal