This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24100 charges properly but doesn't change STAT2

Other Parts Discussed in Thread: BQ24100

Dear TI chargers support staff,

We use BQ24100 to charge a 2500mAh Li-Po battery in one of our products. The battery charges properly (CC and CV cycles have been logged many times and are correct) however once the battery is charged STAT1 changes from low to high state as intended but STAT2 remains high.

This is the actual BQ24100 configuration that we have:

- 5V supply voltage.

- RSET1 10K

- RSET2 2K

- TTC cap 0.1uF


What is most likely to be the cause of this issue?


Best regards,


Luis Olvera.