Hi all,
I implemented the attached LM2611 design, which is similar to the figure 26 in the datasheet. Unfortunately it doesn't work: it shorts the input 12V power upon powerup - the current raises to the 500mA current limit of the lab power supply and the voltage drops from 12V to 2V..
I couldn't find any netlist error or board routing error - note that all the wiring seen in the layout are on top layer.the second layer is GND and the bottom layer is 12V.
The jumper JP11 is not populated.
Thanks for any help.