Please let me know the PFC for toem-pole.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Peter-san,
Why does TI's PFC EVM has two inductors?
I had see in TI's document to one inductor PFC topology.
(www.ti.com/.../slyt650.pdf)
One power device maker published a PFC EVM.
(www.transphormusa.com/.../Totem-Pole-PFC_TDPS500E2C1_0.pdf)
It uses the TMS320 and one inductor PFC.
I think , if to use the UCD3138, should be able to design an one inductor PFC.
Our customers are hoping that the PFC-IC for totem-pole is sold.
Because, they don't want to modify the firmware for each model.
Thanks,
Nagai