This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to calculate R1, C4 Value in TPS63020 for improved load transient performance.

Other Parts Discussed in Thread: TPS63020

Hello,

How to calculate R1 and  C4 Value which is given in Application circuit of datasheet for TPS63020 for improvement of load transient performance.

Thanks.

  • The value of R1 and C4 depends on several parameters, like the feedback resistor network, transfer function of the control loop and more. I would suggest to start with the given values in the datasheet (R1=68kR, C4=4.7pF) and go into an optimization process until the transient response fulfils your requirements. Please note, that a too big capacitor can cause unstable behavior.
    Best regards, Felix