Other Parts Discussed in Thread: TPS3700
Hello,
I'm trying to use TPS3700 as a window comparator (instead of LT6700 from Linear). I've got a question regarding maximum input range. During normal operation, maximum input voltage will be below 5,85 V, so it's included in recommended input range. But during system fault (short circuits in external cabling) input voltage could be as high as 13,7 V, but there is a series resistor of 2,4 kOhm between a connector and IC input pin (so current will be limited to approximately 6 mA). Is it safe to use TPS3700 in such a manner or could it damage the IC?
regards,
Jakub