Dear all,
Could you teach me two questions?
Q1; Can I control CTRL pin by ON/OFF from MCU I/O pin?
Is there no care point?
Q2;Can I consider the efficiency as about 85% at following situation?
I set ILED=102mA (RSET=2ohm, Vin=3.5-4.2V).
*I did not guess the efficiency because the efficiency characteristic is under ILED=20mA at data sheet.
**I attached my application circuit.
Best regards,