Dear, Sir.
My customer is looking foir the bi-derectional load switch to be capable for USB OTG.
Battery charge with 5V power supply output IC is located. The load switch will be set
in front of the IC. Once the system become "Host", 5V VBUS must be output for the
"Device", so di-directional function is required considering USB OTG.
There is a parasitic diode inside of TPS25926. That seems the device could be work
under reverse direction.
1. I wonder TPS25926 could work & no problem for bi-directional usage?
2. If no, Please let me know the bottle-neck or risk.
For instance the limit of parasitic diode forward current, etc.
Best Regards,
H. Sakai