Hello everyone.
Yesterday I let battery(57,4Ah Li-ion with bq3060 integrated in batterypack) to discharge to lowest voltage it can. Today I wanted to see the accurate voltage with EV2300, but got and error that EV2300 doesn’t recognize the device. Afterwards I tried to communicate with BQ3060 through my microcontroller(I used Live variables in my IDE to see values it reads from BQ3060) and it was all incorrect and strange values, for example voltage 5.6, temperature 315 etc.
Afterwards I tried to use EV2300 and microcontroller on other battery which is also 57,5Ah Li-ion with BQ3060, but EV2300 didn’t recognize it too and my microcontroller didn’t read anything.
Is it possible that I could have damaged BQ3060 with electrostatic-discharge from my body when I touched SMBus wires?
This week I have started to feel electrostatic discharge every time I touch water tap.
Thanks in advance.