I'm working on an application that would take 48V in and generate 5V at the output. The input supply is +/- 5% meaning it could stray to 50.4V, slightly higher than the recommended operating conditions. The max is listed as 65V but do I have a guarantee of how the part will respond to a 50.4V input voltage?