From section 9.1.1 of the datasheet;
"The peak inductor current is used in current mode control and to maintain a good signal to noise ratio it is recommended that the peak-to-peak ripple current is greater than 75 mA for dependable operation."
For my application, I need to be able to handle nominal LED string currents down to around 100mA. A 75mA ripple seems quite significant when the nominal current is only 100mA. I was wondering if the 75mA applies only at higher currents (since this IC is rated for currents up to 2A), and can be relaxed for lower nominal currents?
Does the ripple current requirement depend on the value of the current-sense resistor that is used? For instance, a higher sense resistor value would give a larger voltage ripple at the ISENSE pin for the same current ripple. Can the ripple requirement perhaps be expressed in terms of volts at the ISENSE pin, instead of LED current?
Any clarification that can be provided on the ripple requirement would be much appreciated! Thanks.